Featured Products:
CAP Pumping Plant Fire Protection System Upgrade Project
Water is one of Arizona's most precious resources and the Colorado River satisfies much of the demand. To meet that demand, the 336-mile-long Central Arizona Project (CAP) aqueduct annually delivers approximately 1.6 million acre-feet of Colorado River Water to cities, Indian Tribes and Farms in Central and Southern Arizona. The CAP consists of 15 pumping plants that lift the water approximately 2,400 feet from the Colorado River to south of Tucson.
When originally built in the 1970s, these pumping plants were protected by conventional fire alarm systems in compliance with the existing codes. As a member of OSHA’s Voluntary Protection Programs (VPP), CAP felt the Life Safety of its employees warranted the expenditure to upgrade with today's advanced intelligent fire protection technologies.
Project Scope
Chasse Building Team was selected by CAP as the Construction Manager at Risk (CMAR), which sub-contracted CopperState Fire Protection of Phoenix, Arizona to provide solutions from NOTIFIER by Honeywell.
“It was time to take the 30-year-old systems in to the twenty-first century,” said CopperState General Manager Tim Snow.
According to Telma Reyes, CAP Contracting Officer, the upgrade included, “the installation of clean agent fire protection systems, wet pipe suppression systems, fire detection and alarm systems and an upgrade of existing CO2 systems. We modified existing damper systems and existing stairwell pressurization systems as well. Louvered doors were also replaced with solid panel doors. We prepared as-built drawings of all changes and additions.”
CopperState retrofitted four plants, installing new addressable fire alarm systems with a NOTIFIER NFS2-3030 intelligent fire alarm control panel at the head end of each system. As one of the fire industry’s largest capacity fire alarm control panels, it can support up to 3,180 addressable devices and includes a modular design for easy expansion and tailoring.
Standardization of the systems across the plants is an operations and maintenance goal that was definitely obtained by the versatility of the new systems, according to CAP Senior Project Manager Michael Pierce.
“We started out with a cookie-cutter design for each plant, but quickly found out each has its own idiosyncrasies,” Pierce said. “You need to know your system and pay close attention to details, especially in the design review phase.”
Although the purpose of the upgrade was improved life safety, protecting the pump motors, CAP’s biggest assets, was a major objective. Four of the CAP pumping plants located in central and western Arizona are of similar capacity and design. Each plant has 10 pump units of various sizes ranging from 1,500 to 9,000 horsepower each. Each unit is protected by its own High Pressure CO2 fire suppression system, which is monitored and controlled by an NFS2-640 or NFS-320 intelligent fire alarm control panel from NOTIFIER. All fire alarm panels are networked with the main NFS2-3030 panel to allow monitoring, response and maintenance.
Because these pumping plants were constructed with concrete walls up to 48" thick, rigid conduit raceways were installed by the CMAR for the fire alarm cabling used to transport high-speed data between the new NOTIFIER fire alarm control panels via the NOTI-FIRE-NET intelligent fire alarm network. While each panel operates independently, this exclusive networking solution ties all panels together for easy monitoring of the entire network from one or multiple locations over hundreds of miles. The autonomous operations of each panel means the loss of one will not bring down the entire network, resulting in greater survivability.
The plants motor rooms utilize NOTIFIER Acclimate Plus detectors, an intelligent device that uses a combination of photoelectric and thermal sensing technologies for increased immunity to false alarms. Unlike traditional intelligent detectors, the Acclimate Plus has a microprocessor in the detector head that processes alarm data. As a result, the device adjusts its sensitivity automatically, according to the environment, and without operator intervention or control panel programming.
Intelligent devices, such as the Acclimate Plus detector, utilize the patented FlashScan communication protocol, which was developed to speed communication between control panels and analog intelligent devices.
To protect the fire alarm controls in this industrial environment, CopperState customized industrial grade Hoffman NEMA 12 enclosures for many of the panels. The enclosures allow local maintenance staff to view alarm system status easily. They can simply open the NEMA enclosure and manually perform actions, such as alarm acknowledgement and reset.
As a member of OSHA’s VPP, CAP facilities meet or exceed health and safety standards, and maintain injury rates well below National Bureau of Labor Statics rates. Recognition from the VPP encouraged CAP and CopperState to look well-beyond mandates by code.
“We required a lot of extensive testing and had to make a number of changes throughout the installation process,” says Craig Truax, CAP Electrical Controls Engineer. “If you’re going to take on a project of this magnitude, having a contractor that’s competent and willing to go the extra mile to meet your requirements is important.”
Monitoring & Maintenance Made Easy
One of the most evident changes was the improvement in communication of alarms between the CAP headquarters in Phoenix, Ariz., and the four upgraded CAP plants.
The NOTIFIER ONYXWorks graphic workstation allows facility management and security personnel to view the status of all fire alarm and fire suppression networks throughout the four pumping plants. Through CAP’s existing Ethernet infrastructure, the ONYXWorks graphic workstation receives data from each plant’s fire alarm network twenty-four hours a day, seven days a week over IP, allowing CAP personnel to view all system points, alerts and alarm events in real-time. Utilizing the graphic workstation, each plant’s system can be controlled remotely as well.
“Our facilities are so remote that coordinating the communications of alarms is key,” states Justin Larsen, CAP Lead Project Mechanical Engineer. “By avoiding having personnel drive hours to check on a plant, this centralized system will save a lot of labor when it comes to monitoring and maintaining these systems.”
In conjunction with the monitoring centralization of all plant fire protection networks, CopperState configured CAP’s ONYXWorks workstation to serve as a single source of control and supervision for the execution of:
Additional fire protection consulting, inspection and certification services were provided by Rolf Jensen & Associates, Inc. of Phoenix, Arizona. All fire alarms, sprinkler supervision and CO2 systems were tested for compliance to NFPA 13 and NFPA 72 standards.
Potential Advancements
The fire alarm and suppression systems at the remaining 11 CAP plants are scheduled to be upgraded over the next four years. Due to the simplification of fire alarm monitoring and control that CAP has gained through the NOTIFIER ONYXWorks system, CAP has planned for one workstation to be installed at each plant.
Once all 15 plants and Headquarters are upgraded, CAP plans to broaden the scope of its NOTIFIER network to also serve as an emergency communications/mass notification system. Through the ONYXWorks platform, authorized CAP personnel will have the ability to broadcast messages to all or specific areas of a facility using audio and visual notifications; send distributed recipient messages such as emails and computer pop-ups; and even broadcast announcements for miles outside of the plant.